Issue
Adding a Trend to a controller and an error comes up saying that the memory is full
Environment
I/NET Seven Site
Cause
memory full error when adding a Trend to a controller
Resolution
Follow these steps to trouble shoot and see if it will resolve itself.
- Check the memory on the PC and controller itself to see if the error is valid.
- Check the masking etc. on the points as well as the Trend Extension for the correct cell number.
-
If you are still unable to add then please contact Product Support to receive a script that will allow you to add the Trend.