VideoXpert: Standalone VideoXport Player Minimum Specification:

Issue

The minimum specification is needed to select a client system for the export player

Product Line

Pelco Video Management

Environment

  • VideoXpert
  • Export Player

Cause

This information is currently missing from the VideoXpert specification sheet

Resolution

  • Hardware:
    • Dual Core i5 2.67 GHZ
    • 4 GB RAM
    • 200+ GB of free HDD space or more (may not need this much free space)
    • GPU that supports OpenGL 3.0 or higher
    • 1024 x 768 or higher screen resolution  
    • 100/1000 Ethernet Network Interface Card
    • Sound Card

 

  • Software
    • Windows 7 Pro or Ultimate 64 bit or higher
    • .NET 4.6.1 or higher
    • OpenGL 3.0 or higher
    • Direct3D 9 or higher