Optera OSD (On-Screen Display) text or overlays may interfere with the analytics algorithms

Issue

Optera OSD (On-Screen Display) text or overlays may interfere with the analytics algorithms.

Product Line

Pelco Video Management

Environment

Optera

Cause

OSD (On-Screen Display) text or overlays may interfere with the analytics algorithms.

JIRA ticket SPS-6404

Resolution

Here are a couple of possible resolutions to handle this situation:

Option #1

Disable all OSD text and overlays before using analytics.

Option #2

Draw an exclude zone that covers the overlay area.