What Fingerprint readers does Security Expert support?

Issue

What Fingerprint readers does Security Expert support?

Product Line

SmartStruxure Solution, Other

Environment

Security Expert

Fingerprint Reader

Cause

Require information on what Fingerprint Biometrics  are supported with Security Expert.

Resolution

We only officially support Suprema Biometric readers (HLI p/n SX-BIO-SP) however our reader expanders/controllers should be able to be connected/work with any reader that outputs a standard 26bit Wiegand output.
 
If there is a fingerprint reader that does this it should be able to be connected to Security Expert like a standard card reader supplying the controller with Wiegand data that is assigned to a user’s fingerprint. The enrolling of fingerprints etc would need to be handled by the third party system, we would essentially be treating it as a normal card reader and card. 
 
The integration with Suprema Biometric readers allows you to enrol the users fingerprints to the biometric device from within the Security Expert UI.
 
The following fingerprint readers are currently qualified with Security Expert.
 
 
The integration with Suprema Biometric readers allows you to enrol the users fingerprints to the biometric device from within the Security Expert UI. We are actually currently in the process of updating our integration to support a newer version of Suprema readers but the current software supports the V1 Bio Entry Plus readers.We only officially support Suprema Biometric readers (HLI p/n SX-BIO-SP) however our reader expanders/controllers should be able to be connected/work with any reader that outputs a standard 26bit Wiegand output. If there is a fingerprint reader that does this it should be able to be connected to Security Expert like a standard card reader supplying the controller with Wiegand data that is assigned to a user’s fingerprint. The enrolling of fingerprints etc would need to be handled by the third party system, we would essentially be treating it as a normal card reader and card. 
 
The integration with Suprema Biometric readers allows you to enrol the users fingerprints to the biometric device from within the Security Expert UI. We are actually currently in the process of updating our integration to support a newer version of Suprema readers but the current software supports the V1 Bio Entry Plus readers.