Spectra Enhanced Environmental reboots after self-test.

Issue

Environmental Spectra Enhanced is rebooting with the heater off and blower on.

Product Line

Pelco Cameras

Environment

  • D6230 Series
  • D6220 Series
  • Cisco 2960

Cause

The camera is receiving insufficient power

Resolution

With the heater off and blower on, the Spectra Enhanced camera requires 18W of power. Enabling Cisco LLDP and turning off CDP will allow the switch to negotiate the port's POE+ power to 18W.