13M series of lenses are not compatible with Next Generation Sarix Enhanced II box camera

Issue

Larger sensor used in the Next Generation Sarix Enhanced box camera

Product Line

Pelco Cameras

Environment

13M2.2-6
13M2.8-8
13M2.8-12
13M15-50
YV2.7X2.2SR4A
YV2.8X2.8SR4A                 
YV3.3X15SR4A
IXE11
IXE21
IXE32
IXE12
IXE22
IXE32            

Cause

Sensor size of 13M series does not support larger sensor of Next Generation Sarix Enhanced box cameras.

Resolution

Next Gen models
IXE12
IXE22
IXE32

****can only use the YV series on the models listed above****
 

Below is a list of available YV lens models.

Model                                  Description
YV2.7X2.2SR4A                 LENS 1/2.8 MPIXEL          2.2-6MM
YV2.8X2.8SR4A                 LENS 1/2.8 MPIXEL          2.8-8MM
YV3.3X15SR4A                  LENS 1/2.8 MPIXEL          15-50MM

*Note: New lenses will work with all legacy Sarix Pro and Enhanced (Enh-I) cameras