Premise Installs on Windows OS

Issue

Running Feenics applications on a Windows PC that is not server based

Product Line

AccessXpert

Environment

AccessXpert

Server 2012

Server 2014

SQL 2012R2

Cause

If running a Hosted Instance or on a Premise then a Windows 7 Client Workstation can be used.

However if its a Premise install, then the Application Server must be a Server based machine. If you have done a Premise install on a Windows 7 PC and it works, please note that this is not a supported application. There are upgrades on the software itself that would need to be done and more than likely they will fail if attempted and your system may not function correctly.

Resolution

Only use supported Server based machines e.g Server 2012, Server 2012 R2, Server 2014.