VxPro: How to reimage a VxPro Workstation?

Issue

Software issue with Windows.

Product Line

Pelco Video Management

Environment

  • VideoXpert Professional
    • VxPro Workstation (Dell 7050SFF)

Cause

Windows OS is corrupted.

Need to reinstall Windows on a brand new SSD.

Resolution

VxPro Workstation Recovery process

  1. Upon boot up press F12
    Verify that the Boot mode is set to: LEGACY; Secure Boot: OFF - if it is not please stop here and contact technical support 
  2. Select USB Storage Device
  3. At the prompt select number 1 Restore System to Factory Default and hit enter
  4. After recovery completes, remove USB and reboot system.