How to factory default a IJP Professional Series 2 Micro Indoor Dome

Issue

How to factory default an IJP121 using the hardware button.

Product Line

Pelco Cameras

Environment

  • Sarix Professional Series 2 Micro Indoor Dome
    • IJP121, IJP221
  • Factory Reset

Cause

Reset default settings.

Resolution

Both factory default options will default the IP address back to DHCP, if there is no DHCP server the default IP address of 192.168.0.20/24 will auto assign.

 

Factory Default using the web interface:

  • Login to the web interface using a web browser and the IP address of the camera.
  • Navigate to Settings > System > General Settings
  • Click the Restore All Camera Defaults

     

 

Factory Default using the hardware reset button: