Ops Center: Which Windows Performance settings does Ops Center change?


Upon launch of OCC the following message is displayed: "We detected that your Windows Performance settings are not optimal. Click the button below to apply settings."

Product Line

Pelco Video Management


  • VideoXpert
  • Ops Center


Ops Center has detected that optimal windows settings are not being used.


When clicking Apply, Ops Center configures the following custom Visual Effects settings. If any setting differs from the below image, the warning message will appear. These are visual performance settings that can be changed based on your preference. You can hide the message if you would prefer different settings.