v2.0.1 Patch Release Notes - Product Support Release

Issue

Known Fixes for v2.0.1 Patch VideoXpert 

Product Line

Pelco Video Management

Environment

VideoXpert v2.0.1 Patch Release

Cause

Patch Release Notes

Resolution

Video Xpert.png

VX 2.0-1 Patch

_____________________________________________________________________________________

Release description:

This release includes the following bug fixes:

VMS-11213

Core: Non-Admin Roles are not able to Add Presets

VMS-10899

Ops Center SW: Intel Driver causes crash when disconnecting from EVO Cameras

VMS-11408

Ops Center: No mouse zoom control of D5118 when camera is set to closed authentication

VMS-11218

Update Onvif driver to disable auto-configuration of secondary stream

VMS-11008

Updating to the VX 2.0 suite causes PTZ control of NET55XX streams to be delayed.

VMS-11061

[OCC-Aggregation-VxPro] Download of export file from aggregated VxPro site fails

VMS-10998

aggregated devices from a pro system are removed after a period of time (within 20 minutes)

VMS-11431

Core: Ultimate License does not enable Aggregation Feature

VMS-10704

Excluded restrictions permission doesn't apply to newly added device

VMS-10716

Ops Center: Decoder monitors will flicker roughly 3 times a minute

VMS-10728

Privilege migration: Add missing auto-added restrictions

VMS-10729

Privilege migration: Ensure that child restrictions are a subset (subset if exclude=true) of parent's

VMS-10702

VXS: 500 server error returned on assignments tab after a DB rebuild

VMS-11424

VXS: Large numbers of recording gaps trying to record Axis M3006 camera.

VMS-10783

[Core, Exports] Deleting exports in OCC does not actually delete the physical file from the server.

VMS-10668

[Core, Exports] Exporting is failing to download clips that playback fine in OCC and VLC.

VMS-10725

[ExportPlayer] Player will crash when attempting to perform digital zoom while in 4up mode

VMS-11016

[Galaxy Macau] OCC 2.0 (build 10) BRIX decoder monitor flashes/flickers

VMS-10717

[OCC] Crash during collab tab testing

VMS-11133

export poll time is too slow for OpsCenter progress bar

VMS-10780

permissions: assigning "match parent" to a child with a parent that has an exclusion restriction incorrectly clears the parents restrictions

VMS-10997

removing a remote site can hang forever and never complete

VMS-10795

Need index on PriviilegeDbObject.roleId

VMS-10943

Ops Center: PTZ from mouse cannot make small incremental movements for tracking.

VMS-10996

when aggregating a pro system, count is not being set on the page query on the 2nd and all following pages

VMS-10683

[OCC] tvnserver.exe can use over 100Mbps ethernet sending throughput

VMS-11430

Core: Ultimate License does not enable Aggregation Feature

VMS-10726

clients need a way to see if a child permission is in the matchParent mode for restrictions

VMS-10857

fix potential socket leaks with response.bufferEntity() call

 

VX 2.0-1 Released Software Builds:

Product

Build

Download

Core

2.0.1.10

Link

Storage

2.0.1.14

Ops Center

2.0.13360.78

Vx Player

2.0.13360.78

 

System Minimum Requirements:

Core:

  • Intel i7 CPU 64 bit processor

  • 16GB RAM

  • Windows 7 SP3

  • Windows 2008 R2

  • Windows 2012 R2

Media Gateway:

  • Intel i7 CPU 64 bit processor

  • 8GB RAM

  • Windows 7 SP3

  • Windows 2008 R2

  • Windows 2012 R2 SP1

OpsCenter:

  • Intel i7 CPU 64 bit processor

  • 8GB RAM

  • 120 GB SSD

  • Windows 7 Ultimate

  • Window 10 Pro

CMG:

  • Intel i7 CPU 64 bit processor

  • 16GB RAM

  • Windows 7 SP3

  • Windows 2008 R2

  • Windows 2012 R2