What operating systems is Sigma 4.08 supported to run on?

Issue

Information not available in product documentation.

Product Line

Satchwell Sigma, SmartStruxure Solution

Environment

Computer software

Cause

Documentation not updated to show additional operating systems now supported.

Resolution

Sigma 4.0.8.57, as a front-end user interface, is supported on the following operating systems:

Windows XP Pro Service Pack 3
Windows 7 Professional
Windows 7 Ultimate
Windows Server 2003
Windows Server 2003 R2
Windows Server 2008
Windows Server 2008 R2

Sigma 4.0.8 (build 80 – 89), as an engineering tool for Sigma when transitioned into SBO/EBO Sigma is supported on:

Windows XP Pro Service Pack 3
Windows 7 Professional
Windows 7 Ultimate
Windows Server 2003
Windows Server 2003 R2
Windows Server 2008
Windows Server 2008 R2

Sigma 4.0.8 (build 104 onwards), as an engineering tool for Sigma when transitioned into SBO/EBO system Sigma is supported on:

Windows XP Pro Service Pack 3
Windows 7 Professional
Windows 7 Ultimate
Windows Server 2003
Windows Server 2003 R2
Windows Server 2008
Windows Server 2008 R2
**1 Windows 10
**1 Windows Server 2012


**1 The additional operating systems support is only applicable when Sigma is part of a SBO/EBO installation.
(This confirmation was provided to PSS by R and D).