Configuring Power Up mode in Spectra Mini PTZ dome.

Issue

  • Need the Spectra Mini to move to a preset location after power up.
  • Need the Spectra Mini to start a pattern after power up.

Product Line

Pelco Cameras, Pelco Video Management

Environment

  • Spectra Mini (analog)

Cause

After a power surge the camera does not returns to the position it was left at.

Resolution

Configure Power Up Action

Note: Power Up action settings defines a specific activity to be perform in the event the power to the dome is cycled.

 

  1. Enter the Spectra Mini dome settings by programming preset #95.
     
  2. Scroll down to Dome Settings.

     
  3. Scroll down to Power Up.

     
  4. Adjust the Power Up Action setting by selecting one of the available activities. 

 

 

* The following activities are available:

NONE                       No action

AUTO (default)         The dome resumes its prior activity or direction before the power outage.

AUTO SCAN            Dome starts auto scan operation.

RANDOM SCAN      Dome starts a random scan operation.

Frame Scan             Dome starts a frame scan operation

PRESET 1                Dome goes to preset 1.

PRESET 8                Dome goes to preset 1.

PATTERN 1             Dome goes to pattern 1.

 

Related Article:

Access the program menu (Dome Settings) of a Spectra / Spectra mini, Esprit PTZ camera sending the preset 95 command.

How to program a power up action on Spectra Dome using a KBD300A.

Configuring power up action on Spectra Mini, Spectra IV dome using DS ControlPoint.