Under objects such as Doors and Inputs what is the Commands option used for?

Issue

Under objects such as Doors and Inputs what is the "Commands" option used for?

Product Line

SmartStruxure Solution, Other

Environment

Security Expert

Cause

Unsure how to use the Commands option showing in some of the objects options.

Resolution

These cannot be adapted for general use by installers/integrators. These are mostly used for controller instructions that have been included in the firmware but have not been built into the UI yet, as well as internal testing. Leave these alone unless you have a specific need and theinstructions from Product Support on how to configure the command.