STR800 Series Wall Module wiring details

Issue

Not generally available

Product Line

TAC I/A Series, Field Devices

Environment

I/A series

Field device

Cause

Information not provided with the documentation supplied.

Resolution

 

 

 

The STR800 Series User manual can be downloaded by selecting this link.

The STR800 Temperature Sensor RoHS Certificate can be downloaded by selecting this link.

The STR800 Wall Module Specification Sheet can be downloaded by selecting this link.

Other STR800 documentation is available on the Schneider Download Center.