VideoXpert: How many IP cameras can viewed in Ops Center?

Issue

Wanting to view 10 high resolution IP cameras at once.

Product Line

Pelco Cameras, Pelco Video Management

Environment

  • VideoXpert
    • Ops Center

Cause

There is no matrix on max camera count that Ops Center can support.

Resolution

Ops Center client can support a max of 8 1080p @ 30FPS streams per workstation. If using an Enhanced Decoder this will allow you to add an additional 8 1080p streams.

Examples:

If using an OPS-WKS (single or dual monitor workstation) that max 1080p streams you can view is 8.

If using an OPS-WKS6 (Ops center workation with 5 Enhanced Decoders D9U/D10U) you can view a max of 48 1080p streams.

 

VideoXpert product page