SpectraHDR: Unable to Confirm Security Exception of a Self-Signed Certificate in Firefox

Issue

When using SSL with Firefox, you are not be able to add/confirm security exception.

See JIRA ticket # SPS-6581 for additional details

Product Line

Pelco Video Management

Environment

SpectraHDR

Spectra Enhanced

D6220

Cause

When using SSL with Firefox, you are not be able to add/confirm security exception.

Resolution

When using SSL with Firefox, you must uncheck "Permanently store this exception" in order to "Confirm Security Exception".

 

Please refer to the image below to see where the option is that you must uncheck: