Audible alarms not sounding when there are active alarms

Issue

Audible alarms not sounding when there are active alarms.
A Workspace has multiple tabs for graphics navigation and a tab for Alarm View. If a user is not on the alarm tab when an alarm is activated, the audible alarm is not heard and the user does not know that an alarm has been activated. The audible alarm works when the user navigates to the alarm tab. 

Product Line

SmartStruxure Solution

Environment

StruxureWare Building Operation Workstation 1.9

Cause

The Workspace content does not have an Alarm Pane added. 

Resolution

Edit the Workspace to add an Alarm Pane to the Workspace content. If the user do not wish to display the Alarm View due to screen space etc., configure the Alarm Pane Default visibility to Hidden.