Can you connect to a NET5402R using a web browser?

Issue

Is it possible to access a NET5402R using a web browser?

Product Line

Pelco Video Management

Environment

  • ENDURA
  • NET5402R HD Network Video Decoder

Cause

The NET5402R is not found when using a web browser.

Resolution

No, the NET5402R cannot be connected to or configured using a web browser, must use the ENDURA platform to configure.  This includes an ENDURA system with a Endura Workstation (or VCD) and System Manager minimum.

NET5402R is a purpose build decoder for the Endura platform and is not a standalone product. 

 

For more information refer to the Endura NET5402R-HD High Definition Network Video Decoder Manual