Digital Sentry Software House C CURE 9000 integration.

Issue

Will DigitalSentry support C•CURE 9000 v2.50.

Product Line

Pelco Video Management

Environment

  • DSSRV Series
    • DSSRV/ DSSRV2 v7.12
    • DS Pelco API Bundle v7.12
  • Software House
    • C CURE9000 v2.5
    • Pelco-C•CURE 9000 integration driver

Cause

Third party integration

Resolution

Yes. Software House C CURE 9000 integrates with Pelco VMS. For supported features and minimal system requirements see Pelco Software House Integration documentation located on the Pelco Partner First website. Please refer to Software House Technical Support for assistance with installation and troubleshooting.

  1. DSSRV2 will be running V7.12
  2. DS Pelco API Bundle v7.12 will be installed on DSSRV2 (Only DS Pelco API and DSFrameserverservice installed
  3. You cannot add a Pelco Video Server or a Pelco Video Camera until you add a Video Folder. For instruction go you to Pelco Partner First and download Pelco Software House C CURE 9000 V2.X integration Guide manual.