Presets compatibility on a PT680-24P

Issue

Need a PT680-24P with presets.

Product Line

Other, Pelco Cameras

Environment

  • PT680-24P
  • PT680-24SL

Cause

Unable to program presets to the PT680-24P.

Resolution

The PT680-24P and PT680-24SL are standard medium dutry Pan and Tilt.  No preset options are available on these models.  If a Pan and Tilt with preset options is needed, use the PT680-24P/PP.

NOTE: PT680 Series Pan and Tilts are now   obsolete and no longer available through pelco.

Alternative Pan and tilt that can replace a PT680 Series is a Esprit Series, ExSite PTZ or Spectra IV dome. Product sheet for each one of this units can be found on www.pelco.com.