How to setup user photos so they are shown when accessing through a Door.

Issue

How to setup user photos so they are shown when accessing through a Door.

Product Line

SmartStruxure Solution, Other

Environment

Security Expert

Cause

Unsure how to add photos to users and have them displayed when that user is accessing through Doors.

Resolution

There is an option for User photos in Security Expert and the Photo Id option is included with the base Security Expert license. With this "Photo ID" feature enabled you will see the Photo tab on the User object and will then be able to add photos to your users.

 

1. You can associate a photo to your users in the Photo tab of Users | Users.

 

2. In Monitoring | Setup | Status Page Editor, you can set the Style to Display User Image. Doing this will show the users photo with the access event.