FSFP Selection and installation for FMCI and FUMS units

Issue

No link between fiber media convertors.

Product Line

Pelco Video Management

Environment

  • FMCI-PF!
  • FMCI-PF2
  • FMCI-PF1M
  • FMCI-PF1POE
  • FMCI-PG1POE
  • FMCI-PG1M
  • FMCI-PG1
  • FMCI-PG2
  • FUMS-F series
  • FUMS-G series

Cause

Incorrect FSP modules were installed.

Resolution

Please ensure that “A” and “B” FSFP’s are used when connecting media converters via FSFP.

 

Example: FSFP-AFMM1SC2 transmitter is to be used with the FSFP-BFMM1SC2 receiver or FSFP-EGMM2LC.55 can be used with FSFP-EGMM2LC.55 since the FSFP-EGMM2LC.55 can be use as either a transmitter or receiver.

 

Reference: manual C3924-A: figure 8