3D Mouse Operations Guide for DS ControlPoint

Issue

3D mouse buttons have been mapped to DS ControlPoint

Product Line

Pelco Video Management

Environment

  • 3D Mouse
  • Digital Sentry v7.17 or higher
  • DS ControlPoint v7.17 or higher

Cause

New feature

Resolution

Note: If using ControlPoint on a windows 10 client, download and install the win10 driver from here.

Note: Have the ControlPoint application running before plugging the 3D mouse into the client for the first time.

 

3D Mouse Operation in DS Control Point.

·          -> Button will select live tab from any screen

·        Button “1” will navigate control to System Tree. Now Joystick control is in System Tree side.

·        Joystick control will select Cameras in System tree

·        Button “2” will be used to drag camera to Live screen.

·        Button “3” will be used to select and drag next camera in System tree to Live screen.

·        Button “4” will be used to select and drag previous camera in System tree to Live screen.

·        Joystick control will be used to Navigate cells if the selection is in Live screen

·        control will be used to Enable and Disable PTZ functionality.

·        Joystick will be used to Pan and Tilt operation if PTZ button is enabled.

·        CTRL button will initiate Iris open operation if PTZ button is enabled.

·        ESC button will initiate Iris close operation if PTZ button is enabled.

·        SHIFT button will initiate Focus In operation if PTZ button is enabled.

·        ALT button will initiate Focus Out operation if PTZ button is enabled.

·        FIT button will Toggle 1x1 View in live screen.

·         button will initiate 1 Minute Quick Review in live screen.