POE75U-1UP Compativility with IMP121

Issue

IMP121 fails to power up when connected to a POE75U-1UP.

Product Line

Pelco Cameras, Pelco Video Management

Environment

  • POE75U-1UP
  • IMP121

Cause

Product information.

Resolution

POE75U-1UP Compatibility with IMP121:

 

  • The POE75U-1UP injector was intended for use with the Spectra Enhanced Series but this injector can also be used with other PoE (AF) and PoE+ (AT) devices in the Pelco lineup.
  • Ethernet cables of Category 5 or better are required.

 

Note: Faults with the AC cord or Ethernet cables can cause improper operation.