Interface to Suprema Facestation 2

Issue

Does Security Expert support Suprema Facestation 2?

Product Line

SmartStruxure Solution, Other

Environment

Security Expert

Suprema Facestation 2

Cause

Unsure about Facestation 2 and if this is one of the Suprema Bioentry products that Security Expert supports.  

Resolution

This device has not been specifically tested or qualified with Security Expert but is supported by the same SDK that has been used to integrate with Suprema Bioentry W and W2 Fingerprint Readers so should work.
 
It should behave in a similar fashion to the biometric readers whereby it outputs (or can be configured to output) wiegand data to one of the reader ports. The enrollment will likely have to be done via the Suprema software.