How to connect CM9760-KBD keyboard to CM9760-CXTA.

NOTICE

DISCONTINUED PELCO PRODUCT.
This product has been discontinued. For further information please visit pelco.com/support/discontinued-products

Issue

How to setup CM9760-KBD in direct camera control mode to CM9760-CXTA.

Product Line

Pelco Video Management, Pelco Matrix

Environment

  • CM9760-KBD
  • CM9760-CXTA Coaxitron Translator

Cause

How to connect wiring between CM9760-KBD and CM9760-CXTA.

Set CM9760-KBD for direct camera control mode, 

Dip switch settings on CM9760-CXTA.

Resolution

CM9760-CXTA dip switch settings set for P protocol at 4800 baud rate and parity is Even.

  • Set for P protocol dip switch 3 set to ON
  • Set for 4800 baud rate dip switch 6 set to ON
  • Control ptz cameras dip switch 8 to ON

CM9760-KBD with power block with two RJ45 connections.

  • Straight cable from com port 1 of CM9760-KBD to power block which reads keyboard.
  • Reverse cable from CM9760-CXTA com in port to power block which reads system.

 

Related article LL#9747 How to place CM9760-KBD in direct camera control mode.