What is the part number for the IME series outdoor adapter plate?

Issue

Installing the IME series Sarix camera outdoors.

Product Line

Pelco Cameras

Environment

  • IME Series
  • 4X Electrical Box

Cause

New installation of IME series Sarix camera in an outdoor environment.

Resolution

The part number for the outdoor adapter plate for installation of the IME series Sarix camera is: IMEEBAP-E

 

Outdoor Plate Adapter

 

NOTE: The environmental camera is weather tight, rated IP66 if installed directly to a surface. So, this
mounting plate is optional. However, to comply with Type 4X outdoor rating, one must install the Type 4X
mounting plate. (The Type 4X plate has a dual function to mount to junction boxes, so you can ignore the
additional holes if not installing to a junction box.

 

 

 

NOTE: The environmental camera is weather tight, rated IP66 if installed directly to a surface. So, this
mounting plate is optional. However, to comply with Type 4X outdoor rating, one must install the Type 4X
mounting plate. (The Type 4X plate has a dual function to mount to junction boxes, so you can ignore the
additional holes if not installing to a junction