VXS: Axis Cameras require Stream Profile to be configured on the camera to add properly to VXS


Adding Axis Cameras to VXS

Product Line

Pelco Video Management


  • VXE
  • VXS
  • VXP


If you add an Axis camera to a VXS and the camera does not have a Stream Profile configured, it may not create datasources in VideoXpert and the camera will not work correctly because of that.


A configured Stream Profile is require prior to adding any Axis Camera to a VXS for recording.


1. Prior to adding the Axis Camera, Go to the Web UI of the Camera and ensure that there is a Stream Profile Setting configured as seen below:



2.  Then go to Admin Portal -> Add Axis Camera -> Axis Driver as seen below.