ControlPoint installation error 1904.Module

Issue

While installing ControlPoint an Error 1904 is shown

Product Line

Pelco Video Management

Environment

DS ControlPoint

Cause

Installer was ran from inside the downloaded zip folder.

Resolution

  1. Once the ControlPoint installer is downloaded, unzip the contents to another folder.
  2. Run setup from the new folder.

Note: It is possible to click through these errors and ControlPoint can launch successfully. However, connections to a system may fail.