Using BACnet Service Tool / RoamIO2 in Windows 10

Issue

Installed the tool under Windows 10 but unable to assign a port in the tool's connection settings because there are no ports showing in Windows Device Manager.

Product Line

Andover Continuum

Environment

RoamIO2

BACnet Service Tool

Cause

Windows legacy hardware configuration.

Windows 10 by default does not include the legacy ports.

Resolution

Legacy ports must be added in the Device Manager.

1. Open Device Manager from Windows Control Panel.

2. Select 'Action' then 'Add legacy hardware' or Go to "Start" and type hdwwiz.exe then press Enter

3. Next

4. Next

5. Next

6. Select 'Ports (COM & LTP) then Next

7. Select Microsoft/Standard Serial over Bluetooth link then NEXT

8. Complete the legacy hardware installation, Device Manager will then show the ports.

9. In the Service Tool select the appropriate port.

 

When connection has been established from Windows PC to RoamIO2 device, the bluetooth settings in Windows will indicate 'Connected'  NOTE that if it only indicates paired there will be no data transfer even thoug the blue LED is illuminated on the RoamIO2 device.

(see screen shot below)