EH20-P-H two modes of POE


Switch inside of the EH20-P-H unknown what it does.

Product Line

Other, Pelco Cameras, Pelco Transmission & Power


EH20-P-H series


This POE selection switch will enable or disable heaters.  Here is the temperature spec for each mode.

HPOE: -30C to 55C

POE+: -10C to 55C


The EH20-P-H has two modes of POE (Power over Ethernet).  This can be selected via a switch on the power module located here by Red Arrow


NOTE: A Microsemi 9601G midspan injector (PD-9601G/AC) must be use if HPOE mode is selected.  It will not work properly without this injector.  If POE+ mode is selected, it will disable the heaters and enable the enclosure to work on any POE+ midspan injector or Ethernet switch.  One thing to keep in mind is that, this enclosure doesn’t support LLDP.  The network administrator must go into the POE+ Ethernet switch and force the power to be at 30W if a managed Ethernet switch is used.  Using any of the following midspan injectors that we offer will not need any configuration.  


Indoor PoE

PD-9601G/AC Single-port, HPoE midspan

POE1AT-US, -EU Single-port, IEEE802.3at midspan

POE4ATN-US, -EU 4-port, IEEE802.3at midspan

POE8ATN-US, -EU 8-port, IEEE802.3at midspan

POE16ATN-US, -EU 16-port, IEEE802.3at midspan