Issue
- The DSSRV2 recorder hard restarts and then gets stuck at the message "Reboot and Select proper Boot device or Insert Boot Media in Selected Boot device and press a key_". Power cycling or restarting the unit returns it to operation but then eventually the failure is experienced again. This can happen once every couple of weeks or several times a day.
Product Line
Pelco Video Management
Environment
-
DSSRV2 with Intel 535 series internal SSD drive
- Intel SSD SC2BW120H6
- Intel SSD SC2BW240H6
Cause
SSD feature - DevSleep malfunction
Resolution
The process outlined in this article will resolve issues related to the DevSleep malfunction on Intel 535 series SSD drives, there is no guarantee this process will 'fix' a failed SSD drive as other root cause problems could be at work.
Generally if the unit runs normally after a system restart until the next hard restart with ""Reboot and Select proper Boot device...", then there is a good chance the below process will resolve the issue.
Verify the internal SSD drive hardware
-
Open Device Manager (Win + R key, type in devmgmt.msc)
-
Expand the Disk drives catagory.
-
Verify you see one of the impacted models below:
- Intel SSD SC2BW120H6
-
Intel SSD SC2BW240H6
- If you have one of the impacted Intel SSD drives, follow the below procedure.
Disable the DevSleep feature on the Intel 535 Series SSD drives
-
Restart the DSSRV2 recorder and once logged back into Windows back up the DS configuration settings using DS Backup: http://buildingskb.schneider-electric.com/view.php?AID=9784
Note: For backup purposes only, the firmware update should be non-destructive.
-
Download the following files:
- Rufus 2.18 : https://schneider-electric.box.com/s/fer4mt42dsqlwxjk7y94mpueu0xfqyxb
- issdfut_2.0.15.iso: https://schneider-electric.box.com/s/7hfaulgm6dbim7enlq8rxkt78i9jp1qm
-
Flashing Firmware on Intel 535 Series Drives Instructions: https://schneider-electric.box.com/s/qsq8aib5bgl00vtmgfcedlpje1blld6a
Note: The flashing firmware instructions PDF linked above also provides links to download Rufux and the ISO file, if downloaded above you can skip Steps 1 and 2.
-
Follow the instructions outlined in the "Flashing Firmware on Intel 535 Series Drives Instructions" PDF to run the firmware update.