VxOpsCenter: When configuring OpsCenter to time sync with a system that is not configured as a time server, OpsCenter may crash

Issue

2.2 OpsCenters can crash if the NTP field is populated with the IP of a server that is running Meinberg as a client

Product Line

Pelco Video Management

Environment

  • VxPro
  • VxOpsCenter
  • meinberg

Cause

Meinberg is not configured as a server

Resolution

The crash has been resolved in OpsCenter 2.3