Commonly used Continuum Card formats

Issue

Common card vendors, types and formats commonly used by Continuum

Product Line

Andover Continuum

Environment

Continuum

HID

Indala

Corporate 1000

Cause

There is a wide range of card formats available. It's necessary to understand the most commonly used options for Continuum.

Resolution

Credential Card Format

  • H50932 - Schneider Corporate 1000(35) Format
  • A10202 - Andover 37-bit Wiegand Format
  • 4041X (ASP-ANDINF) - Andover 37-bit Indala Format
  • 40045 (ASP-CSI) - CSI Indala Format

Indala Reader Format (FP3511A, FP3521A)

  • 10723 (ASP-ANDINF-1L) - Andover 37-bit Indala Format
  • 1009X (ASP-CSI-2L) - CSI Indala Format
  • 10022 (ASP 26-bit Wiegand-1L) - 26-bit Indala Format

HID MultiCLASS Reader (9xx Series)

  • 4041X (ASP-ANDINF) - Andover 37-bit Indalat Format

For additional  information on other HID formats, see the following article: http://buildingskb.schneider-electric.com/view.php?AID=5977