VideoXpert Enterprise: Can you change the default client connection network port TCP 443?

Issue

Connecting using Pelco Mobile and would like to change the VxE Core connection port from 443 to something else.

Product Line

Pelco Video Management

Environment

  • VideoXpert Enterprise (VxE)
    • VxCore / CMG

Cause

VideoXpert Enterprise uses TCP 443 for VxCore client connections.

Resolution

At this time the default HTTPS TCP 443 VxCore network port is not changable.  This port is hard coded and cannot be edited.