What is the DSSRV2-080P?

Issue

What are the differences between the DSSRV2-080 and the DSSRV2-080P?

Product Line

Pelco Video Management

Environment

  • DSSRV2

Cause

Need to know what the difference between DSSRV2-080 and the DSSRV2-080P.

Resolution

The DSSRV2-080 is the base unit with no power cords. The country code must be added to include the correct power cable. In the below example this would be the part number for a DSSRV2 with a US power cord.

DSSRV2-080-US

The DSSRV2-080P includes power cords for EU, US, and UK. All other equipment remains the same.