Reader status shows Unknown

Issue

When adding a new reader to a controller, the readers status shows "Unknown" in the hardware tree. 

Product Line

AccessXpert

Environment

Access Xpert Version 2

Hosted & Premise Install

Cause

The newly added reader has not been brought into "Online Mode"

Resolution

From the hardware tree right-click on the reader and select "Online Mode". The reader should now show up as online, and the user should be able to control the door operation. 

 

   **Note - If unable to put the readers into online mode, it is necessary to first make the controller active, as shown below. After selecting this, a reboot of the controller is necessary for the changes to take effect.