Oncam EVO-05 audio input specs

Issue

Customer needs Oncam specs in order to buy a supported mic

Product Line

Pelco Cameras

Environment

  • Oncam EVO-05
  • Audio

Cause

Information is missing from Oncam Spec.

Resolution

  • The built-in audio connecter is mono, but the connected jack type is 3.5 mm stereo jack. 
  • The input is Mic input level and type is mono
    • Connecting a Line level input to this jack will cause distortion because the level is too high.
  • The cable length between the mic and camera should be less than 1 meter long.