Workplace Tech 5.9.x and EcoStruxure Building Operation Workplace Tech Editor use with Visio 2013 and 2016

Issue

Proper handing and preparation of existing .vsd files helps eliminate crashing and lockup of the Visio application.

Product Line

TAC I/A Series, SmartStruxure Solution

Environment

Workplace Tech Editor EcoStruxure 1.9.x and newer.   Workplace Tech 5.9.1 and newer.  Both are affected when using Visio 2013 and Visio 2016

Cause

The product is affected by the version of Visio in use as well as the file size and unused objects in the drawing.

Resolution

Follow this procedure for Workplace Tech files

1.       When using Workplace Tech 5.9.2 with Visio 2013 or 2016, the file has to be opened in “Compatibility Mode” DO NOT CONVERT.

Illustration 1

2.      While the .vsd file is open in Visio, not in Workplace Tech, use the “Reduce File Size” option and select the boxes in Illustration 1&2

Illustration 2

3.      In Visio 2016, after opening the “Inspect Diagram”, (Illustration 3), select the first 3 boxes in the “Reduce File Size” option. (Illustration 4)

Ilustration 3

Illustration 4

4.    Save the file for use in the Workplace Tech Project or to be imported into your AS-P as a .vsd.  Add the “cleaned” file to your project or import in Workplace Tech Editor.  Make sure the Visio 2013 or 2016 is at the most recent Version and build.  You can find this under the file/account/About Visio.  If Version 1802 is available in your Microsoft Office update Channel, use it.  Version 1801 was used in testing. For Visio 2013 Build 15.0.4971.1000  MSO 15.0.5007.1000  was tested (Illustration 5)

Illustration 5