Can I add an NSM5300 to an existing NSM5200 recording pool?

Issue

Adding an NSM5300 to an existing NSM5200 recording pool.

Product Line

Pelco Video Management

Environment

NSM5300 v2.5.x

Cause

Wanting to add an NSM5300 to an existing NSM5200 recording pool.

Resolution

Yes. You can add an NSM5300 to an existing NSM5200 recording pool.

*NOTE: Just like with adding any NSM to a recording pool, it is recommended to only add units to the same pool that are of the same storage capacity.