Enrollment Reader in AccessXpert

Issue

How can users be automatically enrolled into AccessXpert?

Product Line

AccessXpert

Environment

Premise Install

Hosted Instance

Cause

Enrollment readers are not used in AccessXpert. 

Resolution

When a card is read at the Door Reader, it will result in an "Access Denied/Card Pin Not Found" event being generated. This event can then be used to create a new user. Once this user has been created and added to the system, the card will become active and have access to the doors it's assigned to.