Does Endura support the use of the KBD300A or 3rd party keyboards?

Issue

The site would like to use the KBD300A or a 3rd party keyboard with the site's Endura system.

Product Line

Pelco Video Management

Environment

  • Endura

Cause

Site request use of the KBD300A or 3rd party keyboard for PTZ control.

Resolution

Endura does not support the use of the KBD300A or 3rd party keyboards. If a keyboard is needed for use on an Endura system then the KBD5000 would be the supported keyboard.