VxPro: Version Matrix

Issue

Customer has an issue with a specific software and only the software version is provided. We need to know which package was used to install the software.

Product Line

Pelco Video Management

Environment

VxPro

Cause

The VxPro installer comes with VxToolbox, VxOpsCenter and VxPro Server which all have different versions

Resolution

VideoXpert Pro Date Type VideoXpert Camera Drivers VideoXpert Pro Server VideoXpert VxOpsCenter VideoXpert VxToolbox
1.0.0.3085 06/01/2017 Image Version   2.1.0.1148 2.1.13228.9319 1.1.0.1531
1.0.0.3226 06/25/2017 First Release   2.1.0.1222 2.1.13593.15 1.1.0.1696
1.0.2.15 12/01/2017 Patch Release 2.1.0.1338 2.1.0.1338 2.1.15104.104 1.3.0.206
1.0.2.26 01/05/2018 Patch Release 2.1.0.1353 2.1.0.1353 2.1.16020.20 1.3.0.206
1.2.0.158 02/02/2018 Patch Release/ Image Version   2.2.0.401 2.2.1.112 1.3.1.22
2.0.0.90 04/03/2018 2.0 Release   2.2.0.454 2.3.0.1167 1.4.0.515
2.5.0.112 06/26/2018 2.5 Release   2.5.0.131 2.5.0.958 2.5.0.109
2.5.1.6 07/23/2018 2.5 Patch Release   2.5.1.6 2.5.1.9 2.5.1.8