VXPro: Adding an Axis M3046-V camera

Issue

Axis M3046-V has been added to VXToolbox but is not populating in Ops Center camera list

Product Line

Pelco Video Management

Environment

  • VXPro version 2.0.0.90
  • Axis M3046-V version 8.10.1

Cause

The Axis M3046-V camera's h.264 stream profile is missing and needs to be added
 

Resolution

Confirm that the Axis camera is added to VXToolbox and is commissioned before proceeding

  1. Open the Axis camera webpage
  2. In the lower right of the screen click on Settings
  3. Click on the Stream Profiles Icon
  4. Click on the Add button
  5. Enter the name StreamProfile1
  6. Click the dropdown and select Video Encoder h.264
  7. Click Save
  8. In Ops Center, click on the refresh icon

Note:  If the screen resolution needs to be adjusted, click on StreamProfile1 then click on the Modify button.  This typically is the case if the camera image in Ops Center shows black bars on the left and right sides.