Issue
Getting an IDisc Wand to work after an upgrade from I/NET 2.XX to I/NET Seven
Environment
I/NET Seven
IDisc
Cause
Getting an IDisc Wand to work after an upgrade from I/NET 2.XX to I/NET Seven
Resolution
- Go to I/O Server and look at the Peripherals Section, Select the correct type of reader (IDisc) and the COM Port (Com 1 or 2) for communications.
- Go to Access, Options, select the supply card number from reader and check this box. It will probably be grayed out.
- Read a card or IDisc and see what happens. If it is set up correctly it will work, if not recheck the settings.
- Verify that the Individual Option is set for Individual as the selection.