ES6230 Esprit Enhanced IR Lamps with Black Film

Issue

There is a Black Film or Black Covering accross the IR of the Esprit Enhanced.

Product Line

Pelco Cameras

Environment

  • ES6230-12-R2
  • ES6230-12P-R2
  • ES6230-15-R2
  • ES6230-15P-R2

Cause

ES6230 are shipped with a clear film over a black film that is placed over the IR light.

Resolution

The Black covering or film will need to be removed before power is applied to the unit, if this is not done before power is turned on it is possible to bake the film on the ir causing it to be very hard to remove.