Issue
Sub-Lan Interface (SLI) Not Available.
Environment
I/NET site with SLI
Cause
Controller is not available to translate a big card number when it has been read at a card reader. .
Resolution
If you are using Access control and wondered what "SLI Not available" means or how it should be used when setting up Messages on the Door Point, the following description should clear up any misconceptions about it.
"SLI Not Available" means that the controller is not available to translate a big card number when it has been read at a card reader.
This can be set up as a Transaction or an Alarm.
A Transaction will be displayed in the Transaction Window whenever this occurs.
An Alarm will be generated if this is selected but it has to match the settings that are selected for the various Alarm type and distribution masks.