What is the default ip address for Midspan 4, 8, and 16 channel?

Issue

New Midspan installation what is the default ip address.

Product Line

Pelco Transmission & Power

Environment

POE4ATN-US, POE4ATN-EU, POE8ATN-US, POE8ATN-EU, POE16ATN-US, POE16ATN-EU

Cause

Defualt ip address unit will default to.

Address to ping device or find device on network.

Resolution

POE4ATN 4-Port IEEE802.3at Midspan default ip address is 10.0.2.5

POE8ATN/16ATN 8- or 16-Port IEEE802.3at Midspan default ip address is 192.168.1.100