Issues resizing SBO graphic editor frames with Windows 10 Lenovo P51 or T470 laptop.

Issue

Issues resizing SBO graphic editor frames with Windows 10 Lenovo P51 or T470 laptop with a Schneider Electric image.

The following picture shows that the Graphic Editor did not re-filled the screen after resizing either the component/snippet area or the Object/property area, a border can be seen to the right and below the editor’s frame.

Product Line

SmartStruxure Solution

Environment

Lenovo P51 or T470 Schneider Electric imaged laptop.

Cause

Scale and layout:
Microsoft .NET Framework version:

Resolution

1. Scale and layout:

Right mouse click on the desktop and select “Display settings”

Set Scale and layout to 100%

Re-boot computer

 

2. Microsoft .NET Framework 4.7.2:

Download and install Microsoft .NET Framework 4.7.2

(Microsoft .NET Framework 4.7.2. can be downloaded from the Microsoft support site)

Re-boot computer

If these suggestions do not provide a solution or if you would like to provide some other feedback, please contact your local product support entity